Technical FAQs

Ask a Question

What utility do you use to upgrade the firmware on a M580 CPU?

Issue: 
Upgrading firmware on the M580 CPU

Product Line:
M580 PLC

Environment:
Modicon M580, Unity 8.0 Programming

Resolution:
The Unity Loader Utility is used to upgrade the firmware on a M580 CPU.

Was this helpful?
What can we do to improve the information ?