Browse FAQs

What is the S09 option for the E-Flex controller unit?

Published date: 23 March 2020

Issue:
Asking about the S09 option for the E-Flex controller unit?

Product Line:
E-Flex

Environment:
All serial numbers

Cause:
Option card is available in with S-Flex but not the open style

Resolution:
The S09 option in the E-Flex is the End Damper Control.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.