Browse FAQs

Can you read the parameters on the ATV212 drive via Lonworks that do not have a SNVT assigned?

Published date: 23 January 2020

Issue:
Can you read the parameters on the ATV212 drive via Lonworks that do not have a SNVT assigned?

Product Line:
ATV212, ATV61, ATV71

Environment: 
All VFD with LonWork communication

Cause
Communication

Resolution:
To access parameters on the VFD via lonworks that is not available by SNVTs, use the nvIParamCmd  and the nvoParamResp

For more details, please see: ATV212_LonWorks_manual_EN_S1A53848_01.pdf

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.