Browse FAQs

Wiring a ConneXium Legacy switch power plug for use without a redundant power source.

Published date: 03 April 2018

The ConneXium switches support redundant power supplies. If you are not using a redundant supplies and the fault light is on then all you need to do is jumper the two power inputs together. This will turn the fault light off. If this does not eliminate the fault light refer to the Quick Reference Guide for the product.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.