Browse FAQs

Permanent removal of Modbus Plus tap drop cable

Published date: 03 April 2018

Is it possible to remove the drop cable from a MB+ TAP 990NAD23000 assembly and still be connected to the Modbus Plus trunk cable?
Yes... As long as jumpers are installed to replace the physical wiring that the drop cable would have made.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.