Browse FAQs

Does the MBX driver MBPSTAT utility work on a Windows7 64 bit PC?

Published date: 03 April 2018

No.
None of the 64-bit editions of Windows support the use of 16-bit applications, and none of these operating systems permit the Virtual MBX Driver to be installed.
The Virtual MBX Driver allows you to run legacy 16-bit applications, both DOS and Windows, under 32-bit Windows operating systems. Currently the only work around to access the MBPSTAT utility is to install the MBX drivers in a virtual environment.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.