Browse FAQs

What are all the Bypass options for M-Flex enclosures?

Published date: 12 February 2020

Question:
Looking for Bypass options for M-Flex enclosures.
 
Product Line: 
All ATV61/71 with Bypass options in M-Flex

Environment: 
All

Cause:
N/A

Answer To Customer:

Power Circuit R ( Isolation and Transfer- RVAT)- This power circuit consists of isolation and transfer contactors integrated with a reduced-voltage autotransformer starter ( RVAT) as the emergency bypass
Power Circuit S (Barriered Bypass- SSRVS)- This power circuit consists of barriered, compartmentalized enclosure design integrating a solid-state reduced- voltage starter ( electronic soft start) as the emergency bypass
Power Circuit T ( Isolation and Transfer)- This power circuit consists of isolation and transfer contactors to coordinate and connect an external electromechanical combination starter, reduced-voltage starter, or solid-state reduced-voltage starter as the emergency bypass.
Power Circuit W ( Drive Only)- This power circuit operates the motor from the power convertor only ( without bypass).
Power Circuit Y ( Integrated Bypass)- This power circuit operates the motor either from the power converter or from full voltage line power ( bypass mode). The motor can be run in bypass mode in the unlikely event that the power converter becomes inoperative.
Power Circuit Z (Barriered Bypass)- This power circuit operates the motor either from the power converter of from full voltage line power ( bypass mode).  The motor can be run in the bypass mode in the unlikely event that the power converter becomes inoperative.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.