Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Do the Magelis XBTGT or Harmony HMIGTO/GK/GTU/STO/STU ranges offer single-mode fiber optic connection for Ethernet?
Issue
Do the Magelis XBTGT or Harmony HMIGTO/GK/GTU/STO/STU ranges offer single-mode fiber optic connection for Ethernet?
Product Line
Magelis XBTGK/GT, Harmony HMIGK/GTO/GTU/STO/STU
Resolution
The Magelis XBTGT HMI family (as well as the Harmony HMIGK/GTO/GTU/STO/STU range) does not have single mode fiber as an option. These targets only come with a copper connection for Ethernet.
A recommendation would be to use a media converter type switch that has a single mode fiber. Schneider Electric offers a Modicon Standard Unmanaged switch, part number:
MCSESU083F2CS0, which has 6 copper ports and 2 single-mode fiber ports.
Do the Magelis XBTGT or Harmony HMIGTO/GK/GTU/STO/STU ranges offer single-mode fiber optic connection for Ethernet?
Product Line
Magelis XBTGK/GT, Harmony HMIGK/GTO/GTU/STO/STU
Resolution
The Magelis XBTGT HMI family (as well as the Harmony HMIGK/GTO/GTU/STO/STU range) does not have single mode fiber as an option. These targets only come with a copper connection for Ethernet.
A recommendation would be to use a media converter type switch that has a single mode fiber. Schneider Electric offers a Modicon Standard Unmanaged switch, part number:
MCSESU083F2CS0, which has 6 copper ports and 2 single-mode fiber ports.
Did this answer your question?
Explore more
Explore more