Browse FAQs

Are the IP54 NEMA 12 ATV71WD......N4 version drives available?

Published date: 03 April 2018

Issue:
Are the IP54 NEMA 12 ATV71WD......N4  version drives available?

Product Line:
Altivar ATV71WD

Environment:
All

Cause:
Needs to order a ATV71WD..........N4 drive but its not coming up on Q2C.

Resolution:
The NEMA 12 IP54 ATV71WD...........N4 drives are not sold in the USA.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.