Browse FAQs

Does Schneider Electric offer a direct replacement for the Berger Lahr D900 series of drive cards?

Published date: 14 January 2020

No, there is no drop-in replacement available to replace the Berger Lahr D900.xx drive cards.
This includes all versions of D900.  
D900.00, D900.50, D900.51, D900.53, D900.61, D900.62, D900.63.... and all others that are not listed but are part of the D900 family.


Customers must upgrade to Lexium SD326DU25S2
They must also replace the existing stepping motor with a BRS3xxW version
Motors used with D900 drive cards are not compatible with SD326 due to a lower voltage rating of the motor windings.   Example: VRDM3910/50 LNA   
The "N" character in the motor type code designates a motor winding rated for 130v.
Motors used with SD326 have a winding rated for 325v

It should be noted that all frame sizes of motors used with D900 drive cards are available in the Lexium BRS motor family so replacement of the motor will not require any mechanical adaptation.

Contact Schneider Electric Technical Support for assistance with selecting suitable BRS motor when upgrading from D900 drive cards to Lexium SD326.


rev 2-19-18



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.