Browse FAQs

What are some possible reasons why I cannot connect SoMove with my drive?

Published date: 28 March 2020

Issue:
What are the reasons that I cannot connect SoMove with my drive? 

Product Line:
ATV12, ATV212, ATV312, ATV32, ATV61, ATV71
 
Environment:
All serial numbers and models.
 
Cause:
Customer cannot establish communication with ATV320 from SoMove using a USB port and TCSMCNAM3M002P cable.
 
Resolution:
1. SoMove and drivers did not install properly 
    a. Install the latest Somove
    b. Install the latest DTM files
    c. Install the the Schneider Electric Modbus driver
2. Verify communication format settings in SoMove, Device Manager and Modbus Driver

For additional details  Refer to the attached PDF 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.