Browse FAQs

Does the ATV61 and ATV71 come with a graphic keypad?

Published date: 03 April 2018

Issue:
Does the ATV61 and ATV71 come with a graphic keypad?
 
Product Line:
ATV61, ATV71
 
Environment:
All models and serial numbers
 
Cause:
None
 
Resolution:
The ATV61 and ATV71 drives come with the VW3A1101 graphic keypad.  To order a drive without the graphic keypad the part number must have a "Z" on the end. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.