Browse FAQs

Using Access Control on the M340 with ModbusTCP clients.

Published date: 03 April 2018

Controlling ModbusTCP client access to the M340 over Ethernet is achieved in the communication network setup of the Unity Pro project.
  1. Select the "Messaging" tab.
  2. Place a check mark in the "Access Control" box.
  3. Enter all IP addresses that will need access to the M340 through the Ethernet port.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.