Browse FAQs

How to find the default Logging Topics available on the EGX300?

Published date: 20 April 2018

Issue
User wants to know the default Logging Topics available.

Product Line
EGX300

Environment
Setting up device logging on EGX300

Resolution

To view the default Logging Topics on an EGX300 for any device:
  1. Log onto the EGX300 web page (default username = Administrator, password = Gateway)
  2. Click the 'Setup' tab
  3. Click on 'Device List' in the left hand column
  4. Add the desired device type
  5. Click 'Apply'
  1. Click on 'Device Logging' in the left hand column
  2. Click 'topics' in the Customize column for the desire device type
  1. The default Logging Topics for that device type will be listed

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.