Browse FAQs

Do SoMachine controllers support CANopen DS305 layer settings?

Published date: 31 August 2018

Issue:
Do SoMachine controllers support the CANopen DS305 layer settings?

Product Line:
SoMachine

Resolution:
None of our SoMachine controllers supports the LSS mechanism of CANopen as a configurable dialog. 
In general it can be realized by using available libraries within SoMachine like CAA_CanL2.lbrary but it is not recommended to do this due to the fact that these libraries are not validated by Schneider and you could run into conflicts with the CANopen Performance Manager and low level functions of CANopen implemented in the firmware of the controller.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.