Browse FAQs

What is the maximum output current of the ATV61HD30N4?

Published date: 19 February 2020

Issue:
Maximum continuous output current rating of the ATV61HD30N4.

Product Line:
ATV61

Environment:
ATV61HD30N4 only

Cause:
Customer unable to find information in current literature.

Resolution:
The maximum continuous output current rating of the ATV61HD30N4 is 66 amps.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.