Browse FAQs

Can I run a 3 phase BMI integrated motor with single phase power?

Published date: 11 May 2018

Issue:
Can I run a 3 phases BMI integrated motor with single phase power?

Product Line:
Lexium 32i

Resolution:
Unfortnately, there is no way to disable the missing phase detection so we cannot run a 3 phase BMI on single phase power.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.