Browse FAQs

Getting E1100 error on the LXM32 servo drive

Published date: 07 June 2018

Issue:
Getting E1100 error on the LXM32 servo drive

Product Line:
LXM32

Resolution:
E1100 is a "parameter out of range" error. The parameter could be coming from a PLC or an HMI communication with the LXM32 drive and sending an out of range parameter like speed, acceleration, deceleration or position.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.