Browse FAQs

Is it possible to use a pointer in a SoMachine basic operate block?

Published date: 04 September 2018

Yes. You can use an operate block with the following syntax.

For example %MW1[%MW10]:=%MW100
[%MW10] is the pointer.  
The value of %MW100 is move to %MWx, x being the value of %MW10.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.