Browse FAQs

Does the HMISCU6B5/8B5 has open wire detection for the temperature input?

Published date: 04 September 2018

Issue:
Does the HMISCU6B5/8B5 has open wire detection for the temperature input?

Product Line:
HMISCU6B5, HMISCU8B5, thermocouple, PT100, value not going to 0

Environment:


Cause:


Resolution:
The HMISCU does not offer Thermocouple Broken wire detection.

 When the T/C is broken the temperature reading stays the same.  Therefore if the process where the temperature is changing at least 0.1F every so often logic could be written to detect a broken wire detection.

Attached an sample Function Block that could imported in the SoMachine project.  It is monitoring the temperation every 10 seconds and if doesn't see a change a broken Thermocouple bit gets set. If 10 seconds is too sensitive then change it to a longer period of time.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.