Technical FAQs

Ask a Question

What range of capacitor which available ?

Different ranges with different levels of ruggedness are proposed:
• "EasyCan": Capacitors for standard operating conditions, and when no significant non-linear loads are present.
• "VarPlus Can & Box": Capacitors for stringent operating conditions, particularly voltage disturbances, or when a few non-linear loads are present. The rated current of capacitors must be increased in order to cope with the circulation of harmonic currents.
• "VarPlus Box Energy": Specially designed capacitors, for harsh operating conditions, particularly high temperature.
• Capacitors with detuned reactors: applicable when a significant number of non-linear loads are present.

For further information available contact catalog ref.: PFCED310003EN (put in search box) as link below:
https://www.se.com/id/en/
Was this helpful?
What can we do to improve the information ?