{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

How to NTP time sync M580 PLC through BMENOC0311 module ?

***** With the release of Unity Pro v13.0 HF2 and BMENOC03x1.4 firmware 2.12 this can be accomplished using the "Update CPU time with the module:" setting in the NOC. ******

For versions previous to the above, find here attached project backup as a ready solution to time synch M580 CPU through NOC module over NTP.

Note :-
- You need to enable block and pulse time sync variable to sync PLC clock. Refer settings done here.
- Enable NTP time service in DTM browser of NOC module and provide NTP time server IP address.

Attachment(s)