Browse FAQs

Does the BMH servo motor have a fan cooling option kit?

Published date: 31 August 2018

Issue:
Does the BMH servo motor have a fan cooling option kit?

Product Line:
BMH motor

Resolution:
The fan cooling option is available only for BMH1904 (Stack 4) servo motor. 
The motor BMH1904xxxxB is shipped with a fan already installed on it. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.