Browse FAQs

Error E7611 on the LXM32 drive

Published date: 31 August 2018

Question:
What is error E7611 on the LXM32 drive?

Product Line:
LXM32

Resolution:
Error E7611 means the resolver is inoperative due to one or more of the following reasons:
- Very long resolver cable between the drive and the motor
- Resolver is inoperative and motor needs to be repaired/replaced
- Bad or no shield on resolver cable
- High power cable running very close to the resolver cable

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.