Browse FAQs

Why does the ATV212 drive have "hello" stuck on the main screen?

Published date: 19 June 2018

Issue:
Why does the ATV212 drive have hello stuck on the main screen?

Product Line:
ATV21 and ATV212 including the S-flex enclosed drives

Environment:
All 

Cause:
Main control board appears to corrupt 

Resolution:
Reseated the control board and its still stuck in hello 
Push mod and it will show AUF then back to hello 
The Main control board appears to be corrupt and the Drive will need to be replaced.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.