Browse FAQs

Why can't I see valid input data on Quantum analog inputs referenced to %IW1 - %IW8?

Published date: 29 June 2018

One possible reason is that Unity uses 8 IO Scanner Health words located at %IW1 - %IW8. Go to the Unity Browser and then to the Communication folder, there under the IO Scanner tab you will see the Health word assignments. You are free to change the starting %IW reference and valid analog input data should begin to appear on %IW1 - %IW8.


R-120517


Legacy KB System (APS) Data: RESL211860 V1.0, Originally authored by DaSo on 06/21/2013, Last Edited by DaSo on 06/21/2013
Related ranges: Modicon Quantum

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.