Browse FAQs

Does Schneider Electric offer a replacement for Berger Lahr motor RECM374/4 D024 5SH 0AS 105 with ID number 18002000184?

Published date: 21 May 2018

The RECM374/4 D024 5SH 0AS 105  with ID number 18002000184 has been obsoleted
The replacement is 0018002000870 which is now known as a BDM7442S0166.

This is a brushless DC motor which is not offer by Schneider Electric in North Amercia.
Customers must contact the OEM machine buiilder for spares using the new part number BDM7442S0166.

Rev 5-21-18

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.