Browse FAQs

What is the allowable voltage range for the Conext SW?

Published date: 30 March 2018

Issue:
Customer is looking for clear voltage limits for the Conext SW. Wants to avoid damaging the unit.

Product Line:
Conext SW Hybrid Inverter/Chargers (2524, 4024, 4048)

Environment:
Any Conext SW installation with an AC source

Resolution:
The unit will only run at 280VAC MAX. It might not qualify right at that limit either since fluctuations can trip it over. AC support will not work at such a high voltage. The inverter can't overcome the high grid. In non-operating mode, the inverter can withstand over 300V L-L.

Cause:
Customer may not be fully clear on AC voltage limits after reviewing spec sheet
Stated: 95-135VAC, 170-270VAC

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.