Browse FAQs

What is the maximum number of Ethernet networks that can be configured for a M340 ?

Published date: 03 April 2018

Title
Maximum number of Ethernet networks that can be configured for a M340 
 
Issue
Maximum number of Ethernet networks that can be configured for a M340 
 
Product Line
M340 BMXNOE0100 BMXNOR0200H
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The maximum number of Ethernet networks that can be configured for a M340 is three Ethernet networks defined in a M340 Unity program.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.