Browse FAQs

Is there delay that can be added to the start signal for ATV61/71 drives?

Published date: 28 February 2020

Issue:
Is delayed Start available on the Altivar 61 or Altivar 71 VFDs?

Product Line:
Altivar 71, ATV71

Environment:
All

Cause:
NA

Resolution:
Yes, but with a limited time adjustment.
L1-  [LI1 CONFIGURATION]
L1d  [LI1 On Delay]
 0 to 200 ms
Factory Setting  0


This parameter is used to take account of the change of the logic input to state 1 with a delay that can be
adjusted between 0 and 200 milliseconds, in order to filter out possible interference. The change to state 0
is taken into account without delay.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.