Browse FAQs

Can RealStream receive information (current, voltage, power, etc.) from 3rd party drives connected over Modbus?

Published date: 25 June 2018

You can use other brands of drives, but there are limitations – you can’t communicate over Modbus. You would have to establish direct connections using analog inputs and outputs. This then limits that amount of I/O that you will have available for the rest of the system. Support for reading device information from 3rd Party drives/starters is coming in a future release.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.