Browse FAQs

Does the RealStream Lift Station support sanitary sewage overflow monitoring and logging?

Published date: 25 June 2018

Yes, this information is logged locally to the controller in both the event log display as well as the internal log. The RealStream Lift Station will alarm on the condition and the start and stop times are logged. This only measures an overflow float at this time, as cases where a flow meter is used are rare.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.