Browse FAQs

Are the 8940 Pump Panels available with a non-fused disconnect?

Published date: 24 August 2020

 Issue:
Trying to order an 8940 pump panel, but they do not want incoming overload protection. 

Product line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8940 Type S NEMA starter pump panels

Cause:
Application adjustments

Resolution:
The 8940 panels are provided as Service Entrance rated devices.  As such, they are required to use overload protection on the incoming power wires.  If non fused entry is desired, consider using a 8538 Combination starter.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.