Browse FAQs

What are the terminal markings for the LUA1C20?

Published date: 24 August 2020

Issue:
LUA1C20 Terminal markings difference

Product line:
IEC Contactors and Starters

Environment:
Tesys U U-Line Auxliary contacts

Cause:
The part has two contacts, which do different functions.

Resolution:
LUA1C20 has a NO fault contact and NO auxiliary contact.

Terminals 97-98 are the normally open Fault signalling contact.  They will close in Short circuit or Overload condition.
Terminals 17-18 are the normally open auxiliary contacts.  They will close in Ready, Run and Overload trip positions.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.