Browse FAQs

ATV212 SFLEX no output voltage with a run command?

Published date: 26 February 2020

Issue:
Why is there output voltage from the SFLEX drive, but not at the motor?  

Product Line:
SFD212

Environment:
SFLEX with Bypass 
:
Cause:
No voltage to the motor

Resolution:
Check the OL relay to see if it is tripped. 
A1 BC and A1 DOC, both measure 120Vac because there is no ground at A2 .
No path No neutral/ground, OL relay is open.
Reset overload.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.