Indonesia (English)

Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website, for company information.

Choose another country or region

  • young girl wearing headphones jumping on bed

    Perangkat Listrik untuk Rumah Anda

  • ulti main image ULTI ULTI is for those who seek the haute couture in space design. With its ultra-clean lines, sleekly chic square profile and instantly identifiable round dollies, ULTI blends two contrasting geometries to create a modern simplicity of unprecedented freshness. The design also offers the maximum scope to showcase the synergy of colour, material and finish in a standard-sized wall plate.
    • ulti main image
    • ulti silver glass 2 gang
  • neo main image NEO Based on art deco and tech-chic, NEO is a breakthrough in switch design. It demonstrates horizontal thinking, with unconventional horizontal dollies and layered details, and is the first mechanical switch to use LED locators and indicators. This is the forward thinking switch for forward thinking people.
  • dimmer main image ZENcelo Inspired by the fully-flat design trend that has transformed everything from airplane seats Inspired by the fully-flat design trend that has transformed everything from airplane seats and TVs to mobile phones and electric stoves, ZENcelo mechanical switches are ideal for interior design concepts that call for switches to be as unobtrusive as possible.
  • pieno main image Pieno Pushing the boundaries of switch design by maximizing the jumbo dolly with slim edges, Pieno maintains an overall slim profile, despite the jumbo dolly, thanks to the innovative SS Mechanism and patented PerfectFace® Switch Architecture. These two innovations also enable quick and high quality installation on any wall surface.
  • s-classic main image Classic With pure uncluttered styling and subtle lines, designed to be in multigang modular mechanisms, Classic has been a firm favorite for long. Made in impact resistant polycarbonate, Classic guaranteed to stand the test of time with an exceptional product life. Tough, resilient and built to take hard knocks are all good reasons to make it a classic switch.
  • vivace main image Vivace Inspired by the influential Bauhaus movement, Vivace expresses a pleasing form following function. With a slim and trim profile, the sleek clean lines and subtle curves manifest a simple, elegant minimalism. Every piece in this robustly constructed range sits perfectly within the context of any modern interior design. Vivace, a style of modern simplicity that is always within your reach.