Indonesia (English)

Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website, for company information.

Choose another country or region

  • young girl wearing headphones jumping on bed

    Perangkat Listrik untuk Rumah Anda

  • DLT wallpates ulti 4gang DLT Wallplates
    Schneider Electric’s DLT Wall Switches feature “Dynamic Labeling Technology”, providing labels that show what each button does. What’s more they change automatically to indicate the status of 
    whatever they are controlling, such as different radio stations, light levels, even if your alarm is 
    armed or not. A Wiser home is an easy home!
    • DLT wallpates ulti 4gang
    • ulti main image
  • ULTI Range glass color tuch screen Wall-mount touch screens
    These C-Touch Touch Screens provide the ultimate control of your home, all from one central point. You can see what lights, music or appliances are on or off at a glance, and then operate them all from the press of the screen. With a C-Touch Colour Touch Screen, you can even control your iPod or Windows Media Player! Available in a range of colours and designs to suit any décor.
    • ULTI Range glass color tuch screen
    • ulti main image
  • 奥智 Zigbee 5场景手持遥控器 Scene Control Systems Scene control systems are used to control different light sources simultaneously, allowing different combinations of light sources to be switched on or off to the pre-set brightness. You can recall your pre-set scenes at one-touch of a button with wireless control available. There are two types of scene control systems: the 2-wire TruRetrofit that directly replaces the existing 2-wire mechanical switches, offering scene control without the hassle of rewiring; and the interoperable control system that suit situations where the whole house rewiring is done, providing more scene options and compatible with upgrades to home control system.