Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
arrow2_left Main Page arrow2_right Geo SCADA Mobile
thumbnail

Geo SCADA Mobile

The efficient way of monitoring and controlling your Geo SCADA system remotely.
Geo SCADA Mobile, coupled to Geo SCADA, a Schneider Electric product, provides remote access to data within your SCADA system, allowing users to monitor performance while on the move. It also improves staff productivity and enhances overall system performance: an easy way to add value to your organisation!
Fully compatible with ClearSCADA. Use GeoSCADA Server to take advantage of new features.
Alarms and Events
  • Alarm actions such as acknowledge, disable and enable. Actions logged to the Geo SCADA event journal.
  • View alarm and event lists.
  • Alarm notification.

Mobile Displays
  • Summary data displays for at a glance understanding of system performance.
  • Available as a shortcut from alarms or database hierarchy, where configured.

Database
  • Browse the Geo SCADA database.
  • View object status at any level.
  • Display filtered alarm and event lists based on database hierarchy.

Data Visualization
  • Display historic data trends for points. optimized for mobile connectivity.
  • Display custom database queries. useful for Key Performance Indicators (KPIs).

Controls
  • Perform controls on selected points in the Geo SCADA database.
  • Actions logged to the Geo SCADA event journal.

User Favorites
  • Customize the app for easy retrieval of your commonly used views.

Security
  • Integrated security with Geo SCADA.
  • Additional security measures for communications outside of the SCADA firewall.

Location
  • Update your user location in ClearSCADA (Requires ClearSCADA 2017 R1)

Search Database
  • Search the database's objects by object name. From the resultset, navigate back into the database to view events, alarms, status information and select Mobile Methods.

Mobile Methods
  • Configure object methods on the Geo SCADA server, to be selectable on the mobile app and/or ViewX client.

Contact your local Schneider Electric sales channel to provide this functionality for your Geo SCADA system(s).
NOTE: This application does not communicate directly with the Geo SCADA server, so additional software is required to enable this. The additional software can be found on the Geo SCADA installation media.

Close

action_close

Also available on...

Size iOS: 2 MB / Android: 2 MB
Price Free
Languages English

Scan QR codes with your phone