Indonesia (English)

Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website, for company information.

Choose another country or region

  • Default Alternative Text

    Air Distribution and Containment

    Hot and cold air containment systems designed to maximize cooling predictability, capacity, and efficiency

  • Read

    • Read more about Schneider Electric solutions

      White Paper #40
      Cooling Audit for Identifying Potential Cooling Problems in Data Centers

      The compaction of Information Technology equipment and simultaneous increases in processor power consumption are creating challenges for data center managers in ensuring adequate distribution of cool air, removal of hot air and sufficient cooling capacity. This paper provides a checklist for assessing potential problems that can adversely affect the cooling environment within a data center. Read White Paper #40
    • Read more about Schneider Electric solutions

      White Paper #130
      Choosing Between Room, Row, and Rack-based Cooling for Data Centers

      Latest generation high density and variable density IT equipment create conditions that traditional data center cooling was never intended to address, resulting in cooling systems that are oversized, inefficient, and unpredictable. Room, row, and rack-based cooling methods have been developed to address these problems. This paper describes these improved cooling methods and provides guidance on when to use each type for most next generation data centers. Read White Paper #130
    • Read more about Schneider Electric solutions

      White Paper #68
      Cooling Strategies for IT Wiring Closets and Small Rooms

      Cooling for IT wiring closets is rarely planned and typically only implemented after failures or overheating occur. Historically, no clear standard exists for specifying sufficient cooling to achieve predictable behavior within wiring closets. An appropriate specification for cooling IT wiring closets should assure compatibility with anticipated loads, provide unambiguous instruction for design and installation of cooling equipment, prevent oversizing, maximize electrical efficiency, and be flexible enough to work in various shapes and types of closets. This paper describes the science and practical application of an improved method for the specification of cooling for wiring closets. Read White Paper #68
    • Read more about Schneider Electric solutions

      White Paper #153
      Implementing Hot and Cold Air Containment in Data Centers

      Containment solutions can eliminate hot spots and provide energy savings over traditional uncontained data center designs. The best containment solution for an existing facility will depend on the constraints of the facility. While ducted hot aisle containment is preferred for highest efficiency, cold aisle containment tends to be easier and more cost effective for facilities with existing raised floor air distribution. This paper investigates the constraints, reviews all available containment methods, and provides recommendations for determining the best containment approach. Read White Paper #153
    • Read more about Schneider Electric solutions

      White Paper #50
      Cooling Options for Rack Equipment with Side-to-Side Airflow

      Equipment with side-to-side airflow presents special cooling challenges in the modern data center. Common rack enclosures and rack layouts are fundamentally incompatible with side-to-side cooling, resulting in equipment that receives supply air of excessive temperature. This paper describes the problem along with several side-effects that are not generally appreciated. Various solutions to the problem are described along with their costs and benefits. Read White Paper #50
    • Read more about Schneider Electric solutions

      White Paper #123
      Impact of High Density Hot Aisles on IT Personnel Work Conditions

      The use of modern enclosed hot aisles to address increasing power densities in the data center has brought into question the suitability of working conditions in these hot aisle environments. In this paper, it is determined that the additional heat stress imposed by such high density IT environments is of minimal concern. Read White Paper #123
    • Read more about Schneider Electric solutions

      White Paper #135
      Impact of Hot and Cold Aisle Containment on Data Center Temperature and Efficiency

      Both hot-air and cold-air containment can improve the predictability and efficiency of traditional data center cooling systems. While both approaches minimize the mixing of hot and cold air, there are practical differences in implementation and operation that have significant consequences on work environment conditions, PUE, and economizer mode hours. The choice of hot-aisle containment over cold-aisle containment can save 43% in annual cooling system energy cost, corresponding to a 15% reduction in annualized PUE. This paper examines both methodologies and highlights the reasons why hot-aisle containment emerges as the preferred best practice for new data centers. Read White Paper #135
    • Read more about Schneider Electric solutions

      White Paper #182
      The Use of Ceiling-Ducted Air Containment in Data Centers

      Ducting hot IT-equipment exhaust to a drop ceiling can be an effective air management strategy, improving the reliability and energy efficiency of a data center. Typical approaches include ducting either individual racks or entire hot aisles and may be passive (ducting only) or active (include fans). This paper examines available ducting options and explains how such systems should be deployed and operated. Practical cooling limits are established and best-practice recommendations are provided. Read White Paper #182
    • Read more about Schneider Electric solutions

      White Paper #199
      How to Fix Hot Spots in the Data Center

      Data center operators take a variety of actions to eliminate hot spots. Some of these actions result in short term fixes but may come with an energy penalty and some actions may even create more hot spots. Airflow management is an easy and cost effective way to permanently eliminate hot spots while saving energy and can avoid the capital expense of adding more cooling units. This paper describes the root cause of hot spots, recommends methods to identify them, reviews the typical actions taken, and provides the best practices to eliminate them. Read White Paper #199
    • Default Alternative Text


      InfraStruXure® Solution Helps Colocator Deliver 100% Uptime

      "Not only does it address current needs, InfraStruXure’s modular nature enables maximum scalability. The InfraStruXure installation is light-years ahead of other data center power and air equipment installations I’ve experienced." Read InfraStruXure® Solution Helps Colocator Deliver 100% Uptime
    • Small Data Centre


      InfraStruXure® Solution Prevents Energy Company Meltdown

      "There is nothing else on the market like it. I have worked in conventionally cooled environments, and the efficiency of the InfraStruXure solution makes it far and away the best solution I have ever worked with." Read InfraStruXure® Solution Prevents Energy Company Meltdown
    • Technician at data center, data center management, data center operations


      APC by Schneider Electric Precision Cooling Enables Server Deployment Options

      "The Hot Aisle Containment System is unique in that it has enabled us to change our thinking on server installations. APC’s total solution... adds value because we are able to manage server placement, power, and cooling consumption at a detailed level." Read APC by Schneider Electric Precision Cooling Enables Server Deployment Options
  • Learn

    Trade-off Tool: Data Center InRow™ Containment Selector


    Trade-off tool that shows the impact of preferences and constraints on the recommended containment approach. Data Center InRow™ Containment Selector

    EcoAisle Containment


    Hot and cold air containment systems designed to maximize cooling predictability, capacity, and efficiency at the rack, row or room. EcoAisle Containment

    Cooling Solutions for IT Equipment


    Right-sized systems for every environment, from network closets to data centers. Cooling Solutions for IT Equipment

    NetShelter SX Solutions for Cisco Nexus 7000 Series Networking Switches


    Product brochure and part number guide for the Side Airflow Duct Solution and enclosures for the Nexus 7000 Series level. NetShelter SX Solutions for Cisco Nexus 7000 Series Networking Switches

    NetShelter SX Solutions for Cisco Catalyst and MDS Networking Switches


    NetShelter Networking Enclosures featuring Airflow Duct Kits. NetShelter SX Solutions for Cisco Catalyst and MDS Networking Switches

    Vertical Exhaust Duct (VED) for NetShelter SX Quick Reference


    The Vertical Exhaust Duct (VED) System is a low cost easy to install solution that mounts to the top rear of NetShelter enclosures to capture and return hot exhaust air to perimeter cooling systems. Vertical Exhaust Duct (VED) for NetShelter SX Quick Reference

    If you’re not using some type of containment system in your data center, you’re likely sacrificing about a 30% improvement in cooling system performance, this podcast explains why. Boost Cooling System Performance with Containment Systems

    This blog details six potential air containment solutions you can choose between to save energy. Six Air Containment Solutions Will Help You to Save Energy in Your Existing Data Centers

    Which is best for an existing facility – hot air or cold air containment? Hot or Cold Air Containment? Examine Your Constraints to Decide

    Three typical approaches to deploying ceiling-ducted air containment. Did You Choose the Right Ceiling-ducted Air Containment for Your Data Center?
  • Watch

    • EcoAisle: Flexibility Meets Innovation

      The EcoAisle system delivers the most flexibility within a standard product, making it the best choice for both cold and hot aisle containment. View the video to see what else EcoAisle has to offer.
    • US Cooling Capabilities for the Data Center and Beyond

      An out-of-date, inefficient cooling system has a significant impact on your bottom line no matter what business you're in. Schneider Electric can upgrade your facility with a full range of Business-wise, Future-driven cooling solutions that are scalable, flexible, reliable and efficient.