{}

FAQ Pencarian

{"searchBar":{"inputPlaceholder":"Cari berdasarkan kata kunci atau ajukan pertanyaan","searchBtn":"Cari","error":"Masukkan kata kunci pencarian"}}

What is the reference of Type A or Type B thermostat in Prisma Plus switchboard ?

Article available in these languages: Finlandia, Indonesia, Thailand

Type C thermostat is available in Prisma Plus, the part reference of which is 08998. The Type C thermostat Reference 08998 can be used as Type A or Type B by carrying out the modification in the settings and cabling.
For making the thermostat Type A or Type B, connect load on the terminal 2 instead of terminal 3 and the supply at L and N. See figures attached for details.






Lampiran

1.jpg1.jpg [12.62 KB]
2.jpg2.jpg [59.33 KB]

Apakah ini bermanfaat?

Jelajahi lebih lanjut
Produk:
03033
Jelajahi lebih lanjut
Produk:
03033