Bagaimana kami dapat membantu Anda hari ini?

What is the maximum power consumption of ECI850 IEC61850 Sepam server?

Issue
The power consumption specification of the ECI850 is required.

Product

ECI850 Communication Server

Sepam Protection Relays

Environment
IEC 61850 communication environments
Sepam systems using ECI850
Substation automation networks

Cause
The customer needs to know the maximum power consumption value for sizing, design, or integration purposes.

Resolution
The maximum power consumption of the ECI850 is 4 W. This value should be considered when performing system design calculations, panel sizing, or power budgeting in substation automation applications.