Emergency Action Plan

    When disasters strike, restore power and operations as quickly as possible

  • Solutions

    Having a detailed emergency action plan can limit the financial and personal havoc they can cause. Schneider Electric engineers can help you create an emergency action plan to help restore power and normal operations as quickly as possible.
  • Value Proposition

    Emergency action plan components include:

    • Have a current single-line drawing of the electrical distribution system

    • Identify which electrical equipment is critical to the electrical infrastructure

    • Determine which equipment must be replaced and that which can be reconditioned, if water damage has occurred.
Default Alternative Text

Applications

Explore More Ways Schneider Electric Services Can Help

Our nationwide network of professional engineers and qualified field representatives is available any time, for any brand of equipment. If your electrical system has been damaged by a disaster, call 1-888-778-2733

Benefits

  • Default Alternative Text
    Single point of contact 24-hour access to our manufacturing plants
  • Business people in hard-hats walking on factory floor with lots of machines, power management, plant solutions.
    Services available for a broad range of electrical equipment, including other manufacturers.
  • Default Alternative Text
    National network of service locations and factory-trained service representatives.
Nos conseillers sont disponibles pour répondre à vos questions de 8h00 à 18h00 du lundi au vendredi toute l'année.