Schneider Electric, the global leader in energy management and automation, is launching a number of offerings designed to maintain power supply in the event of an outage.
The transfer switch solutions increase power security and availability, as well as reducing downtime by ensuring the supply of power to a building by moving to emergency backup sources, such as generators or batteries, if the primary source goes down.
This means organisations can maintain vital services and avoid business disruption and potential financial losses by keeping essential equipment and operations up and running during a power cut.
The new automatic transfer switch solutions include:
Acti9 Incoming Automatic Transfer Switch Kit
-
A new addition to Schneider Electric’s Acti9 range, equipped with TransferPacT Automatic, providing transfer switching capabilities to an Acti 9 distribution board up to 125A.
-
The transfer switching kit follows the Acti9 design and offers a bolt-on configuration, allowing the option to retrofit onto existing Acti9 equipment
-
It is an off-the-shelf, ready-to-install solution that is provided as an all-in-one kit and includes sensing inputs, monitoring, and control logic for source change-over operations.
ASCO Single Way Bypass Transfer Switch
-
A newly designed switch offering a single-way bypass arrangement. This allows primary power switches to be inspected, tested and maintained without interrupting the supply of power.
-
The new Single Way Bypass ASCO switch offers a current capacity rating from 32A to 400A with IP31 and IP55 ingress protection rating, and is suitable for various applications and conditions.
-
ASCO’s firefighting lift variant ensures that critical applications are able to continue to run efficiently in the event of a fire.
TransferPacT – 32A-1600A
-
With a new frame size, the TransferPacT all-in-one transfer switch solution now offers intelligent transfer switching capabilities between 32A-1600A
-
TransferPacT provides automatic transfer switching as fast as 500ms, as well as best-in-class power availability even in extreme working environments.
-
It has a futureproof design allowing for flexible functionality expansion with swappable function modules.
-
Also offers multiple additional functions, including remote control, load shedding, generator control, fire protection and beyond.
David Williams, Schneider Electric’s Vice President for Transactional Business said: “We are having many conversations with organisations about the need for increased power security and availability as the demand continues to rise putting pressure on the grid at times. Few organisations can afford to be without a steady power supply and for some, such as healthcare providers, it can be a life-or-death situation.”
“Our new transfer switch kits are there to provide peace of mind so that if the primary power source fails it’s easy and quick to transfer over to emergency sources, keeping vital equipment and operations up and running and limiting the impact.”
Related resources:
About Schneider Electric
Schneider’s purpose is to create Impact by empowering all to make the most of our energy and resources, bridging progress and sustainability for all. At Schneider, we call this Life Is On.
Our mission is to be the trusted partner in Sustainability and Efficiency.
We are a global industrial technology leader bringing world-leading expertise in electrification, automation and digitization to smart industries, resilient infrastructure, future-proof data centers, intelligent buildings, and intuitive homes. Anchored by our deep domain expertise, we provide integrated end-to-end lifecycle AI enabled Industrial IoT solutions with connected products, automation, software and services, delivering digital twins to enable profitable growth for our customers.
We are a people company with an ecosystem of 150,000 colleagues and more than a million partners operating in over 100 countries to ensure proximity to our customers and stakeholders. We embrace diversity and inclusion in everything we do, guided by our meaningful purpose of a sustainable future for all.
Discover the newest perspectives shaping sustainability, electricity 4.0, and next generation automation on Schneider Electric Insights
Hashtags: #TransferPacT #TransferSwitches #AutomaticTransferSwitch #ATS