Browse FAQs

What is the difference between an ATV61H.... and an ATV61K.....?

Published date: 08 April 2020

Issue:
Drive nameplate shows ATV61H…. the drive menu 1.11 shows ATV61K …

Product Line:
Altivar 61

Environment:
All
 
Cause:
Different part numbers for the same drive.

Resolution:
Example: ATV61HU55N4 (IP20) is on the nameplate, but in the Drive menu (1.11 IDENTIFICATION) shows ATV61KU75N4 (IP00).
When the open style IP20 is changed to IP00, the drive rating increases by one size and the identifying part number changes from H (shown on drive nameplate) to K (shown in the drive menu).  Based on UL test results, the rating change can only be done in our offering of enclosed packages, such as MCC M-Flex and E-Flex.  IP00 is not an option for an open style drive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.