{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What are the differences between the ATV31 and ATV312?

Issue:
ATV31 vs ATV312 drive.

Product Line:
ATV31, Altivar 31, ATV312, Altivar 312

Environment:
All models, all serial numbers.

Cause:
ATV31 became obsolete in Dec 2010.

Resolution:
The ATV312 drives are a direct replacement for the ATV31 drives (or ATV31-A). Please see attachment. The ATV312 drive has the same dimensions, wiring, and programming as the old version ATV31 drive.

The changes made from the ATV31 to ATV312 include:
-  Optional DeviceNet, Profibus, CanOpen Daisy Chain communication cards.
-  Addition of a rotary dial to quickly scroll parameters
-  Addition of Run/Stop buttons
-  Addition of a door to cover the buttons against accidental contact
-  changed the color of the plastic to follow Schneider Electric color coding (white = control section, black = power section)

Attachment(s)

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.