{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the SIS LABEL software, part number XBY2U, run in Windows Vista?

The "SIS Label" label creation software for Harmony XB4 and XB5 pushbutton controls has been qualified for use with Windows XP and earlier.

The XBY2U software has not been validated for use in a Windows Vista environment.

The pack supplied under part number XBY2U comprises:

  • CD-ROM with the SIS Label label creation software
  • 9 assorted sheets of precut self-adhesive labels for printing
  • 7 templates, corresponding to the various types of label sheets (sold separately)

These templates correspond to the following label types:

  • ZB6YA013, ZB6YC013, ZB6YD013,
  • XVBCY2, XVBCY1,
  • ZBY1101, ZBCY1101, ZBY4100, ZBY5100.

The templates are used to check that the texts are centred before they are printed.
Sheets ZBY4100 and ZBY5100 come with backing boards and covers to ensure the labels are correctly positioned in their holders (e.g. ZBZ32 & ZBZ33).

Please note that this software is no longer available, it was made obsolete in 2016 with no replacement.
Later windows Computers have access to the XP virtual machine , which may run the old software, but please note that the interface drivers from the software to the printer would need to be tested to make sure that the windows software chipset does not block the output of the printer.

This old system has now been replaced by an on line customisable tool for the pushbutton ranges available thought the Schneider electric web site under the pushbutton page. Customization page in the configurator tool

Schneider Electric Ireland