{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is the replacement part number for Lexium 05 drive bearing part number LXM05BD22N4?

Issue: Replacement


Product Line: Lexium 05B


Environment: None


Cause: Obsolescence


Resolution:
The corresponding part number to replace a LXM05BD22N4 will be a LXM32MD18N4 in terms of current rating. Lexium 05B is a Profibus drive and hence the option card VW3A3607 needs to be ordered as well. Importing the GSD file for the Lexium 32 in the PLC program and some configuration changes at the drive are to be expected. Profibus command structure between Lexium 05B and Lexium 32 is very similar and so it should not call for significant programming changes. Some programming changes are to be expected.

Schneider Electric Ireland

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.