Regarding the Energy Rollout settings, the default value for the ION7350 is 10,000,000 but this value can be increased anytime using ION Setup, open the setup assistant and navigate to Basic Setup > Rollover. The limit for this register is really high so you can set to up to 999,999,999 if needed
Note: The ION7300 meters are no longer for commercialized in the UK. The alternative is the ION9000 range. See link below.
NEW! PowerLogic ION9000 | Schneider Electric UK (se.com)
Note: The ION7300 meters are no longer for commercialized in the UK. The alternative is the ION9000 range. See link below.
NEW! PowerLogic ION9000 | Schneider Electric UK (se.com)
Released for: Schneider Electric Ireland