{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Osisense XM - What is the adapted pressure switch XMLBS35R2S11SCQ?

The adapted pressure switchXMLBS35R2S11SCQ is the standard pressure switch XMLBS35R2S11, having the following factory settings : PH = 0.27 bar,  PB= 0.18 Bar. Logistic situation in December 2021: available to order without any marketing restriction; MTO product (MTO = manufacture to order). XMLBS35R2S11SCQ data sheet = XMLBS35R2S11 ones, attached

Attachment(s)

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.