{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Will the SR2MOD03 work with a 3G network?

Issue:
Will the SR2MOD03 work on a 3G network?

Product line:
Twido, M221

Cause:
The SR2MOD03 will not work on a 3G network.

Resolution:
The SR2MOD03 is compatible with 2G and 3G network.


Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.